LPC4357 + SDRAM (MT48LC8M32B2B5-6 ) interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4357 + SDRAM (MT48LC8M32B2B5-6 ) interface

1,660件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Prabhakaran_Raja on Mon Feb 08 21:14:55 MST 2016
Hi,

I have LPC435x-Xplorer++ board.
I need to interface LPC4357 with SDRAM(MT48LC8M32B2B5-6) over EMC.
i'm using LPCXpresso v7.9.2 IDE.
so can any one suggest me Is there any example or library available for SRAM interface. (over EMC)  
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,461件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

Please check the below application note, this appnote describes how to properly interface SDRAM memory to the LPC1800 and LPC4300 External Memory Controller.

AN11508: SDRAM interface to LPC18xx/43xx EMC | www.LPCware.com

I hope this helps


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,461件の閲覧回数
moller
Contributor II

Did you find a solution? I would be very interested in any help and info I can get my hands on to interface to my 64MB SDRAM.

0 件の賞賛
返信