LPC4337 JTAG Not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4337 JTAG Not working

2,523 次查看
danny_tom
Contributor I

Hi,

on a new designed board with LPC4337 microprocessor we have serious JTAG problems and it seems the impedance on the JTAG pins of the CPUs is not correct (one pin, the SWIO/TMS has an impedance of 50 KOhm, and the others SWDCLK/TCLK, SWO/TDO, NC/TDI is approximately 1.1 MOhms). We had one previous design with LPC4337 CPU which works fine and we had no problem with the JTAG, the impedance on all the pins SWIO/TMS, SWDCLK/TCLK, SWO/TDO, NC/TDI is approximately 1.6 MOhms. We made many boards with both design and in the first lot we had no problem but in the second lot all the CPUs have the same JTAG problem. We use the same company to solder the both boards (both LPC4337 quad flat and BGA) so there should be no problem coming from soldering. The layout is approximately identical, only that the new board design has Ethernet connection and the old board did not had Ethernet. The Ethernet design is exactly the same NGX Xplorer board which works fine! So we are wandering what can cause this JTAG problem on our new design? Can be that in the new board all the CPUs have a fabric problems with the JTAG pins?

best regards

D. Toma

标签 (1)
0 项奖励
回复
2 回复数

2,243 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

You might also want to take a look at the FAQ: https://community.nxp.com/message/630601 

Regards

LPCXpresso Support

0 项奖励
回复

2,243 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Toma daniel,

   I found there has a similar question in our community, please refer to that recommend at first:

JTAG not working on LPC4337 

  You can use a new board, then just solid the smallest system, the JTAG interface, and don't add the Ethernet circuit, then use the above link's recommendation, then test it again.

If you still have question after use that recommend, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复