LPC4337 IAP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4337 IAP

1,289 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by GH on Wed Mar 12 06:36:44 MST 2014
Hi,

i am trying to use IAP features to access the flash of a LPC4337 device.

The device offers multiple commands to prepare the flash for write and erase operations:

Cmd 49: Init IAP
Cmd 50: Prepare sectors for write operation

Is it necessary to call both commands prior to each write access or is it sufficient to call "Init IAP" command once after a system reset?

Best Regards
GH
Labels (1)
0 Kudos
Reply
1 Reply

1,235 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Wed Mar 12 15:06:22 MST 2014
Hi,

Yes it is necessary to use both the commands - Init IAP and Prepare sectors.


Thanks,

NXP Technical Support
0 Kudos
Reply