LPC4337 : I want a sample of SPIFI by SGPIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4337 : I want a sample of SPIFI by SGPIO

1,170件の閲覧回数
atsuyosano
Contributor I

LPC4337 : I want a sample of SPIFI by SGPIO

タグ(1)
0 件の賞賛
返信
2 返答(返信)

997件の閲覧回数
atsuyosano
Contributor I

Thank you.
Camera interfaces may be near.
If there is an example of the CLOCK output parallel data output, please tell me.

0 件の賞賛
返信

997件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Unfortunately we don't have an example like you need, however you can use the below application notes as reference.

http://www.nxp.com/documents/application_note/AN11351.zip?fasp=1&WT_TYPE=Application%20Notes&WT_VEND... 

http://www.nxp.com/documents/application_note/AN11343.zip?fasp=1&WT_TYPE=Application%20Notes&WT_VEND... 

http://www.nxp.com/documents/application_note/AN11196.zip?fasp=1&WT_TYPE=Application%20Notes&WT_VEND...

http://www.nxp.com/documents/application_note/AN11275.zip?fasp=1&WT_TYPE=Application%20Notes&WT_VEND...


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信