LPC4078 LQFP100: SPIFI + SD card at the same time?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4078 LQFP100: SPIFI + SD card at the same time?

775件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gjwep on Wed Apr 01 14:24:23 MST 2015
Hello,

I am using LPC4078 LQFP100 and I'd like to use SPIFI and the SD card interface. 

Per datasheet, the only pin that has SPIFI_CLK (P0.22) is also the only pin which has SD_DAT[0]. Is there a smart workaround to still be able to use both peripherals at the same time?

Any hints much welcome.

Thanks in advance,
gj
ラベル(1)
0 件の賞賛
返信
0 返答(返信)