LPC4078 LQFP100: SPIFI + SD card at the same time?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4078 LQFP100: SPIFI + SD card at the same time?

765 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gjwep on Wed Apr 01 14:24:23 MST 2015
Hello,

I am using LPC4078 LQFP100 and I'd like to use SPIFI and the SD card interface. 

Per datasheet, the only pin that has SPIFI_CLK (P0.22) is also the only pin which has SD_DAT[0]. Is there a smart workaround to still be able to use both peripherals at the same time?

Any hints much welcome.

Thanks in advance,
gj
Labels (1)
0 Kudos
Reply
0 Replies