LPC3250FET296: i2c bus hang

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC3250FET296: i2c bus hang

3,034件の閲覧回数
kimran
Contributor I

Hi ,

I am using a custom board based on LPC3250FET296 . It is running Linux 3.18 kernel.

I am seeing i2c bus hangs with the following messages:

Jan 1 01:43:58 (none) user.err kernel: i2c-adapter i2c-1: Master timed out. stat = 2a60, cntrl = 000e. Resetting master...
Jan 1 01:43:58 (none) user.err kernel: i2c-adapter i2c-1: PNX4008-I2C1: Bus busy. Slave addr = 40, cntrl = 0, stat = 2a60
Jan 1 01:43:58 (none) user.err kernel: i2c-adapter i2c-1: PNX4008-I2C1: Bus is still active after xfer. Reset it...
Jan 1 01:43:58 (none) user.err kernel: i2c-adapter i2c-1: PNX4008-I2C1: Bus is still active after xfer. Reset it...
Jan 1 01:43:58 (none) user.err kernel: i2c-adapter i2c-1: Master timed out. stat = 2a60, cntrl = 000e. Resetting master...
Jan 1 01:43:58 (none) user.err kernel: i2c-adapter i2c-1: PNX4008-I2C1: Bus busy. Slave addr = 40, cntrl = 0, stat = 2a60
Jan 1 01:43:58 (none) user.err kernel: i2c-adapter i2c-1: PNX4008-I2C1: Bus is still active after xfer. Reset it...
Jan 1 01:43:58 (none) user.err kernel: i2c-adapter i2c-1: PNX4008-I2C1: Bus is still active after xfer. Reset it...
Jan 1 01:43:59 (none) user.err kernel: i2c-adapter i2c-1: Master timed out. stat = 2a60, cntrl = 000e. Resetting master...
Jan 1 01:43:59 (none) user.err kernel: i2c-adapter i2c-1: PNX4008-I2C1: Bus busy. Slave addr = 41, cntrl = 0, stat = 2a60

After googling a bit I found the following thread:

https://community.nxp.com/thread/316813 

This talks about recovering the i2c bus by making the master send 9 clock pulses. I see that some of the i2c controllers have (ST, OMAP etc.) have implemented the recovery mechanism but the recovery mechanism is not implemented for 

Philips-IP3204 I2C controllers.

Just wanted to know if someone has tried this out. From my understanding of the data sheet apparently GPIO functionality is not available for SCL pin here.

0 件の賞賛
返信
1 返信

1,732件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Imran,

As a complementary information regarding the thread that you already found, you could also refer to the following:

https://community.nxp.com/thread/429674

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信