LPC2470 Bootloader issue with Windows10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2470 Bootloader issue with Windows10

1,847 Views
pandiayn8696
Contributor I

Hi , I am using LPC2470 in one of our project and we have developed the usb bootloader for field upgrade . We developed the bootloader based on AN10764 (USB secondary ISP bootloader for LPC24xx ) . It was working well for all Windows platform except Windows 10 . Windows 10 actually identify the device and i could see the folder but not able to open the folder to copy the bin file . 

 

Hope some of you might have faced the same issue and awaits to get a support from experts to solve the issue. 

 

Thanking you , 

 

Pandiyan.

Labels (2)
0 Kudos
Reply
1 Reply

1,782 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Pandiyan,

Hope you are doing well.

Please continue the thread on your other post.

https://community.nxp.com/thread/530717 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply