LPC2387 interface with MM74HC573 - 3 state problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2387 interface with MM74HC573 - 3 state problem

810件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Erez on Thu Sep 24 02:18:16 MST 2015
Hi,
Im using P1[17] as out_control for MM74HC573.
When i first connect the voltage or reset the system, i am getting voltage 2[v] ( ONly voltage above 3[v] means '1')
This is a big problem. i need the value to be '1' (or '0').
How can i solves this?

I've tried some actions:
- Disabled the P1[17]  ENET-MDIO option
- Tried to write directly to the register- no effect
- Tried to connect pull up resistor.

Could someone help in this please?

By the way,
I have already a system that works perfect when i use the P0[26] for outcontrol.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)