LPC2378 and SRAM 621024D-70LL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2378 and SRAM 621024D-70LL

1,046 Views
moacir_silveira
Contributor I

Hi all... My first post... Sry for my english...

I know that LPC2378 is old, I know that SRAM 621024 is old, but i am working with this 2 parts, and need a help.

I work for many year with PIC (18/32) and Arduinos, and now i am starting work with ARM...

I know many things, but i am can't do SRAM and LPC2378 work together. My problem: The EMC configuration not is right... The acces time for this memory is 70ns, and i do this memory work with PIC18F87J50 fine...

Whats happen: I do not know if the problem is in WR or RD operation. After write 65535 bytes, when i will read this 65535 bytes, he stop in addr 1230 or 515 or any other addr, with wrong byte read...

I need help with config in the EMC for memory with 70ns time access. I searched in internet, founded many solutions, for another timings, and I tryed many numbers, any success...

My code is anexed. This code is not final, is only a test:

Cristal 12MHz, PLL 72MHz

Ty a Lot

Moacir Jr.

Labels (1)
0 Kudos
Reply
0 Replies