LPC2378 Failed to autobaud in FlashMagic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2378 Failed to autobaud in FlashMagic

5,743件の閲覧回数
betata
Contributor I

we have designed a board using LPC2378.

when download program using FlashMagic, some boards can download program successly.

but we meet that a number of boards always Failed to download while using the same tool and the same setting.

show"....Failed to autobaud Step1...."

I have try many ways, and now have no idea....

what is the problem? please give me some advice.. 

or can I have any other ways to download program to the LPC2378 chip?

thank you very much!

0 件の賞賛
返信
1 返信

4,902件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi He,

Please refer to the following link, which provides several tips and tricks for the most common troubles related to FlashMagic auto-baud of LPC devices:

Failed To Autobaud 


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信