LPC2148FBD64 BDSL File Download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2148FBD64 BDSL File Download

1,516 Views
antonerasmus
Contributor I

Hi,

 

Where can I download the BDSL file for the LPC2148FBD64 ?

What is the IR len for this device ?

 

Regards

  Anton

0 Kudos
Reply
3 Replies

1,504 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi,

You can request the IBIS and BSDL models in the following page:

Microcontroller Symbols, Footprints and Models | NXP Semiconductors

Pablo_Ramos_0-1743699086199.png

Best Regards

Pablo

 

0 Kudos
Reply

1,497 Views
antonerasmus
Contributor I

Hi,

This does not work.

It opens up another browser when I click on the submit link  with an empty page.

Also I can understand providing this information for future reference, but why could you not submit the request in the first place ?

Regards

  Anton

Tags (1)
0 Kudos
Reply

1,488 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi, 

The standard procedure for requesting a new symbol is for customers to fill the online form so that they receive the requested symbol without intermediaries.

When you press submit you should have two options, browser and email, could you try setting the default application of MAILTO to email and try again?

I recommend you check the following page in order to change the default apps of MAILTO

Set Outlook as default MailTo application | Microsoft Community Hub

Best Regards

Pablo

0 Kudos
Reply