LPC18xx refresh time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC18xx refresh time

1,841 Views
setoh_waituck
Contributor I

Hi all,

hope you can help.

I'm using LPC18xx with MT48LC4M32B2P-6A IT

re the following

/* Keil SDRAM timing and chip Config */
STATIC const IP_EMC_DYN_CONFIG_T MT48LC4M32_config = {
     EMC_NANOSECOND(64000000 / 4096),     /* Row refresh time */

since for automotive part,  the datasheet has indicated trefAT 16 ms max compared with tref 64ms for other options.

https://www.micron.com/parts/dram/sdram/mt48lc4m32b2b5-6a-it

Q.  should the calculation be changed as follows?

EMC_NANOSECOND(256000000 / 4096),     /* Row refresh time */

thanks and rgds,  setoh.

0 Kudos
Reply
2 Replies

1,756 Views
jeremyzhou
NXP Employee
NXP Employee

Hi wt setoh,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
According to the datasheet, the 128Mb SDRAM requires 4096 refresh cycles every 64ms (commercial and
industrial) or 16ms (automotive). About your question, the refresh timer value should be configured as below when using the automotive version.

EMC_NANOSECOND(16000000 / 4096),     /* Row refresh time */


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,756 Views
setoh_waituck
Contributor I

Hi Jeremy,

Thanks for the advice.

rgds,  setoh.

0 Kudos
Reply