LPC18xx and USB Vendor-Specific protocol

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC18xx and USB Vendor-Specific protocol

1,358 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by namorada on Wed Apr 29 08:05:44 MST 2015
Hi everyone,

I'm presently trying to search some example for a USB Vendor-Specifi protocol operation.
Does one of you have any idea of where to find that?

Thanks,

D.
Labels (1)
0 Kudos
Reply
2 Replies

1,315 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by namorada on Sun May 03 23:50:30 MST 2015
Hi,

Thank you for your answer.
In fact, i should use (on the PC) a custom driver (Cypress for CyConsole). As i understand, the usb rom stack is only for standard, isn't it ? I mean CDC, Audio, MSC, ..Or did i misunderstand anything?
0 Kudos
Reply

1,315 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri May 01 07:40:52 MST 2015
Hi namorada,
Do you mean vendor specific class(custom class)?

You can look into USBD ROM stack documentation at
http://docs.lpcware.com/usbromlib/v1.0/struct_u_s_b_d___h_w___a_p_i___t.html
and
http://docs.lpcware.com/usbromlib/v1.0/index.html
0 Kudos
Reply