LPC1820 programming algorithm source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1820 programming algorithm source code

1,408 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vdelabouere on Thu Jan 08 17:43:59 MST 2015
Hi,
Where can I find the most up-to-date software source code for the programming algorithm working on the LPC1820 for SPIFI flash program using the dfusec utility ?
I will need to recompile this algorithm because the flash I use is not supported by the SPIFI library.

Thanks.

Vince
Labels (1)
0 Kudos
Reply
2 Replies

1,382 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vdelabouere on Fri Jan 09 10:15:29 MST 2015
Thanks. Got it.
0 Kudos
Reply

1,382 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wellsk on Fri Jan 09 07:26:02 MST 2015
The full project is part of the LCT installer now. When you install it, the source and project for the programming algo installs with it at c:/program files/nxp/...

http://www.lpcware.com/lpclink2-config-tool
0 Kudos
Reply