LPC17xx USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC17xx USB

920件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by venkatesh on Tue Feb 19 22:24:22 MST 2013
Hi,

im working in lpc1768 for usb as device.
when i load the USBMEM, then its detecting as mass storage device.
so by using usb analyzer, i can see the scsi commands passed in between Host and device.
so i give same command through usb analyzer, its passing the same command to device, but no response in IN endpoint

how can i understand complete code flow..
how can get response from device.where i need to check the code.

Thnaks,
venky
ラベル(1)
0 件の賞賛
返信
0 返答(返信)