LPC1788 with TFT interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1788 with TFT interface

1,639 Views
manikantakuntum
Contributor I

hi,

I am using  LPC1788 controller for interfacing TFT Display. I require to know that what  impedance should the RGB bit lines contains for interfacing with TFT Display and what impedance should i provide for interfacing  CLK signals

 

manikanta.k

Tags (1)
0 Kudos
Reply
1 Reply

1,325 Views
soledad
NXP Employee
NXP Employee

Hello Manikanta.k,

Please check the below link, you will find a schematic file that you can use as reference.

http://www.haoyuelectronics.com/Download/HY-LPC1788-SDK/HY-LPC1788-Core_SCH.pdf

In addition, I'd like to recommend looking at this thread:

http://www.lpcware.com/content/forum/dram-pcb-layout-works-only-60-mhz

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply