LPC1788 sdcard interface drvie eMMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788 sdcard interface drvie eMMC

2,353件の閲覧回数
mini92
Contributor I

I use LPC 1788 SDIO interface driving eMMC but initialization err 

0 件の賞賛
返信
2 返答(返信)

2,036件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

According with the reference manual the LPC1788 supports SD card interface that also supports MMC cards only.
So, this device does not support eMMC.


Have a great day,

Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,036件の閲覧回数
mini92
Contributor I

Hi,

    eMMC and MMC card Hardware interface is same ,different is driver software ,

 

   and MMC card drive  eMMC driver  The difference is very small

 

   Can software not support it?

I see

In fs_mci.c function :

/**
* @brief Read card configuration and fill structure CardConfig.
*
* @param None
* @retval TRUE or FALSE.
*/
Bool mci_read_configuration (void)

/* Select Card */
if(MCI_Cmd_SelectCard() != MCI_FUNC_OK) /* CMD7 tese same card reader */
{
break;
}

//  In this line add achieve:

EmmcReadExtCsd  

and according to ExtCsd message set same CardInfo

Can you help me?

thank you

0 件の賞賛
返信