LPC1788 module with 84MHz CPU / EMC frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788 module with 84MHz CPU / EMC frequency

1,902件の閲覧回数
MarcoAEE
Contributor II

Goodmorning everyone,

we are using from years a LPC1788 module with 120MHz CPU frequency and 60Mhz EMC frequency (32bit SDRAM and NOR FLASH) starting from a quartz 12Mhz. The implemented applications work well, we have more products that use panels with resolutions up to 800x600, communications bus, analog and digital I/O, ecc...

Now we would like consider using 84Mhz for CPU and EMC, we want increase the system performance but also maintaining the robust and reliable system.

We already tested the 96MHz but with complex applications get of HARD FAULT.

The 84Mhz tests are satisfactory pier and everything seems to work.

We know that we are going beyond the specification limit of 80Mhz for EMC. We would like to avoid changing the 12 MHz crystal to 16Mhz for the optimal frequency of 80MHz.

Do you think going 4 MHz more than the allowed limit could give problems that now we do not see? Does anyone already use the system in this way?

Thank you

ラベル(1)
0 件の賞賛
返信
1 返信

1,627件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

We do recommend customer to obey the datasheet requirement about EMC module running with Max. 80MHz clock.

The datasheet required clock frequency  be guaranteed for long term working.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信