LPC1788 lcd display affect capture interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788 lcd display affect capture interrupt

952件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fire on Thu Sep 06 18:27:25 MST 2012
That the use of emwin516, display content by capturing the decoded, only capture a decoding display information, through the capture interrupt display information obtained is correct, as long as the information through the emwin516 interface function display out, capture interrupt is affected, one along the two times to capture interrupt, and capture register(CCR) value is the same as the capture the

ラベル(1)
0 件の賞賛
返信
0 返答(返信)