LPC1788: configuring external SDRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788: configuring external SDRAM

1,531 次查看
giusloq
Contributor III

I'm using SDRAM ISSI IS42S32200L connected to LPC1788. I configured it with the following code in CAS=3:

 

#define CLK0_DELAY     7

Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_EMC);

	/* Setup EMC Delays */
	/* Move all clock delays together */
	LPC_SYSCTL->EMCDLYCTL = (CLK0_DELAY) | (CLK0_DELAY <<  | (CLK0_DELAY << 16 | (CLK0_DELAY << 24));

	/* Setup EMC Clock Divider for divide by 2 */
	/* Setup EMC clock for a divider of 2 from CPU clock. Enable EMC clock for
	   external memory setup of DRAM. */
	Chip_Clock_SetEMCClockDiv(SYSCTL_EMC_DIV2);
	Chip_SYSCTL_PeriphReset(SYSCTL_RESET_EMC);

	/* Init EMC Controller -Enable-LE mode- clock ratio 1:1 */
	Chip_EMC_Init(1, 0, 0);

	/* Init EMC Dynamic Controller */
	const IP_EMC_DYN_CONFIG_T IS42S32800D_config = {
		EMC_NANOSECOND(64000000 / 4096),
		0x01,				/* Command Delayed */
		3,					/* tRP */
		7,					/* tRAS */
		EMC_NANOSECOND(70),	/* tSREX */
		EMC_CLOCK(0x01),	/* tAPR */
		EMC_CLOCK(0x05),	/* tDAL */
		EMC_NANOSECOND(12),	/* tWR */
		EMC_NANOSECOND(60),	/* tRC */
		EMC_NANOSECOND(60),	/* tRFC */
		EMC_NANOSECOND(70),	/* tXSR */
		EMC_NANOSECOND(12),	/* tRRD */
		EMC_CLOCK(0x02),	/* tMRD */
		{
			{
				EMC_ADDRESS_DYCS0,	/* EA Board uses DYCS0 for SDRAM */
				3,			//2,	/* RAS */

				/* Mode Register */
				EMC_DYN_MODE_WBMODE_PROGRAMMED |
				EMC_DYN_MODE_OPMODE_STANDARD |
				EMC_DYN_MODE_CAS_3 |			//EMC_DYN_MODE_CAS_2
				EMC_DYN_MODE_BURST_TYPE_SEQUENTIAL |
				EMC_DYN_MODE_BURST_LEN_4,

				/* DynConfig */
				EMC_DYN_CONFIG_DATA_BUS_32 |
				EMC_DYN_CONFIG_LPSDRAM |
				EMC_DYN_CONFIG_2Mx32_4BANKS_11ROWS_8COLS | 		//EMC_DYN_CONFIG_8Mx16_4BANKS_12ROWS_9COLS |
				EMC_DYN_CONFIG_MD_SDRAM
			},
			{0, 0, 0, 0},
			{0, 0, 0, 0},
			{0, 0, 0, 0}
		}
	};
	Chip_EMC_Dynamic_Init((IP_EMC_DYN_CONFIG_T *) &IS42S32800D_config);

 

Is it correct?

It seems it is working, but I have some issues with certain boards, so I want to be sure this isn't related to SDRAM configured in a wrong way (maybe above some hardware limits).

0 项奖励
回复
1 回复

1,515 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Giuseppe,

I think the so-called CAS=3 means Programmable CAS latency, it is programmed into the MODE REGISTER of SDRAM. The parameter is defined in the

MC_DYN_MODE_CAS_3

or

MC_DYN_MODE_CAS_2

 

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复