LPC1788: best SDCard driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1788: best SDCard driver

1,415 Views
giusloq
Contributor III

I'm going to add SDCard support to my application that will run on LPC1788. I have external SDRAM and the application actually runs emWin (I don't know if this is important).

I know there is LPCOpen demo projects for LPC1788, but they are very old (2014!!). Is there any recent SDcard driver available for LPC1788? Should I use LPCOpen driver?

In the forum I found another driver here, dated back 2015.

Any suggestions?

 

0 Kudos
Reply
2 Replies

1,380 Views
carstengroen
Senior Contributor II

@giusloq ,

I have the mmci driver running you refer to (the one in a rar file) in the posts. I gave up on NXP's original MMCI driver a long time ago. The one by "Wolfgang Muees" in the file "auerswald_lpc178x_mci.tar.gz" has been working here for some years (the code is actually from 2011.

Hope it can help you in some way!

Regards,

Carsten

0 Kudos
Reply

1,391 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

LPC1788 is old product of 8 or 9 years ago. Now NXP only has LPCOpen demo for it.

As I know there is no plan to release new sdcard demo for it.

Have a nice day,

Jun Zhang

0 Kudos
Reply