LPC1788. Static EMC read, but doesn't write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1788. Static EMC read, but doesn't write

1,253 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Qazzaq on Thu Apr 12 11:49:32 MST 2012
Hi everyone, Please, help me solve problem with EMC on LPC1788.
I configure EMC static memory (using LPC1788 188pins, no dynamic memory) and when I read from it everything is fine, but when I write to it there's no WE.
All pins configured rightly, debug shows that everything is normal, CS, data bus and address bus responds correctly, but WE is always high.
My code for EMC is below. Maybe someone has the same problem?

    LPC_SC->PCONP |= (1 << 11);  //11 PCEMC External Memory Controller power/clock control bit.



    /* P3.0-P3.7 - EMC_D[0-7]
   * P4.0-P4.15 - EMC_A[0-15]
   *
   * P4.24 - /EMC_OE
   * P4.25 - /EMC_WE
   *
   * P4.30 - /EMC_CS0
   * P4.31 - /EMC_CS1
   */

    for(i = 0; i < 16; i++)
    {
        if (i < 8) PINSEL_ConfigPin(3,i,1);
        PINSEL_ConfigPin(4,i,1);
    }

    PINSEL_ConfigPin(4,24,1);  //OE
    PINSEL_ConfigPin(4,25,1);  //WE

    PINSEL_ConfigPin(4,30,1);  //CS0
    PINSEL_ConfigPin(4,31,1);  //CS1


    LPC_EMC->Control     = 0x00000001;
    LPC_EMC->Config      = 0x00000000; 

/* Config CS1 and CS0 :
Memory width  8 bit, Page mode disabled
Extended wait disabled, Writes not protected
*/
    LPC_EMC->StaticConfig0 = 0;     
    LPC_EMC->StaticConfig1 = 0;    
Labels (1)
0 Kudos
Reply
1 Reply

1,175 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Karl on Fri Apr 13 06:07:51 MST 2012
Hi,

Try with PB bit (7) = 1 in LPC_EMC->StaticConfigX
0 Kudos
Reply