LPC1788 - SDRAM after a watchdog reset...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 - SDRAM after a watchdog reset...

969 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Marc Crandall on Mon Dec 05 14:29:10 MST 2011
Hello,

I'm using an LPC1788 with a MT48LC16M16 SDRAM chip.  All works well and I do not have any issues with the external memory in normal operation.

I use a bootloader to configure the external memory and run a memory check.  My problem is when I get a watchdog reset in the main application (I'm causing them on purpose for testing) the configuration of the external SDRAM runs in the bootloader and one of two things happens:
1) Everything works exactly the same as on a power up (50% of the time)
2) As soon as I try and access the memory I get a fault that kills my debugger. (The other 50% of the time)

Does anyone have any idea what is going on?  Note I have tried this with SCB bit 1 on/off no difference.  I've also tried not re-configuring the EMC when it's a watchdog reset but this seems to fail every time.

Does anyone know how to safely and surely reset this SDRAM?

Thanks

M
标签 (1)
0 项奖励
回复
0 回复数