LPC1778 USB HOST CDC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1778 USB HOST CDC

1,470 Views
andyyang730
Contributor I

Dear Support

   I need to use USB HOST CDC on LPC1778,do you have example which can share with me ? 

   Thanks for your support.

Best regards

Andy

0 Kudos
Reply
1 Reply

1,314 Views
soledad
NXP Employee
NXP Employee

Hi Andy,

Please check the below thread:

USB Host CDC Example | www.LPCware.com 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply