LPC1778 Programming too slow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1778 Programming too slow

1,878 Views
lorenzogalbiati
Contributor I

Hello,

This is the first time I use LPC1778 and Flashmagic tool for programming.

I have bought USB-ICP-LPC2K programmer.

The programmer works well but I have to set the baudrate at 57600 as maximum speed.

If i set 115200 the autobaud fails.

The programming time is very long ad 57600: about 5 minutes in order to program all the flash.

Have anyone experienced a problem like this?

Are there other faster programmers on the market?

best regards.

Labels (1)
0 Kudos
Reply
1 Reply

1,799 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Lorenzo Galbiati

Please refer the following link to see the programmers that we recommend, you can check the different options to see which adapts better to your needs. 

http://nww.preview.nxp.com/support/developer-resources/software-development-tools/lpc-developer-reso... 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply