LPC1777- Firmwre not downloading through JTAG (JTAG device chain error)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1777- Firmwre not downloading through JTAG (JTAG device chain error)

1,145 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by anandana on Mon Sep 28 19:16:57 MST 2015
Hi,

        I have wrongly downloaded LPC2468 firmware in LPC1777 controller using H-Jtag Programmer. After this I am not able to download LPC1777 firmware using JTAG(ULIMK - ME). I am getting JTAG device chain error. Can someone help me in this. Is there any possibility to erase flash and re program?

Regards
Anandan A
标签 (1)
0 项奖励
回复
3 回复数

1,128 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Tue Sep 29 01:03:18 MST 2015
I am pretty sure that in ISP mode for the 177x/8x family you need to interface via UART 0.

I use 1778 208 QFP and the pins are Port 0/2 and 0/3.

See your user manual about the ISP commands/pin connections -- or just use FlashMagic. JTAG or SWD is not involved here.

HTH Mike.
0 项奖励
回复

1,128 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by anandana on Mon Sep 28 21:56:40 MST 2015
Hi MC,

           Thanks for your reply. I tried the same LOW on pin P2[10] while RESET is LOW. Now I am getting error that  no cortex device found, Check the JTAG or Connection. Please guide me in this.

Regards
Anandan A
0 项奖励
回复

1,128 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Sep 28 20:34:08 MST 2015
Hi AnandD,
Put device in ISP mode and try to erase/program device. A LOW on pin P2[10] while RESET is LOW forces the on-chip boot loader to
take over control of the part after a reset and go into ISP mode
0 项奖励
回复