LPC1764 Vbus&AD04 function question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1764 Vbus&AD04 function question

871件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zhongqiu2015 on Wed Jun 10 04:35:08 MST 2015
LPC1764 have 8 channel ADC input. But the ADC input 4 and the Vbus are the same pin.
Now, I need ues the USB module and 8-channel ADC input at the same time. So, could I ues the USB module without the Vbus pin function? What is the influence about  the USB function whitout the Vbus?
ラベル(1)
0 件の賞賛
返信
0 返答(返信)