LPC175x usb bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC175x usb bootloader

1,273 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by beto on Fri Sep 19 19:10:01 MST 2014
Anyone know if one can add a usb bootloader to the LPC175x that operates similar to LPC1343 internal usb bootloader which comes up as a mass storage device.

Does AN10177  apply to 17xx family also ?  Is there any shortcuts or example code for 17xx?

b/
Labels (1)
0 Kudos
Reply
1 Reply

1,262 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Fri Sep 19 19:23:05 MST 2014
RDB1768 examples are including a complete USB bootloader  :)

http://www.support.code-red-tech.com/CodeRedWiki/RDB1768cmsisExampleProjects

Download:

http://www.support.code-red-tech.com/CodeRedWiki/RDB1768cmsisExampleProjects?action=AttachFile&do=ge...

Just comment out LCD stuff and libraries and it's working...
0 Kudos
Reply