LPC15xx startup time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC15xx startup time

2,145 Views
lak1
Contributor I

Hi

I am using the LPC1518 for a project and I have a problem, that only can be solved with a very short startup time. I need the system to set some GPIO to pull down or just set them low.

I just try with a very simple program, as seen below, which is not fast enough. So if anyone can help me or teach me how this can solve this is would be a big help for me.

int main (void) {

SystemCoreClockUpdate();

Chip_GPIO_Init(LPC_GPIO);
Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_SWM);
Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_IOCON);

Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 31, (IOCON_DIGMODE_EN | IOCON_MODE_PULLDOWN) );

Labels (1)
0 Kudos
Reply
2 Replies

2,107 Views
converse
Senior Contributor V

You need to look in the LPC15xx User Manual to see how long it takes to boot (it is specified) - it may already take too long before your code gets to run.

0 Kudos
Reply

2,107 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Lasse,

If you want to execute an action the fastest possible after the MCU is out of reset, you could try to do it in the startup code, all the LPCOpen examples has an API called SystemInit that is executed before entering the main, maybe you could try adding the initializations you want to this region?

Best Regards,

Alexis Andalon

0 Kudos
Reply