LPC15xx in smaller than QFP packages ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC15xx in smaller than QFP packages ?

1,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cgroen on Thu Dec 17 04:59:44 MST 2015
Not sure if this is the right place to ask, but trying anyway ;)

Are there any plans for releasing LPC15xx devices in smaller packages than the QFP packages (which are mighty big) ?
Labels (1)
0 Kudos
Reply
1 Reply

1,230 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Thu Dec 17 13:43:45 MST 2015
Agreed - HVQFN33 would be nice.
For the LPC13 parts, TSSOP would also be handy - it would be good to have the Cortex M3 instruction set in a small package.
TSSOP makes it easy to wire it up on a single sided board.

Not so important with the LPC15 as it has the switch matrix, and you can put most inputs and output where you want them.
0 Kudos
Reply