LPC15xx SPI ROM DMA example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC15xx SPI ROM DMA example

1,578 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Fri May 27 12:05:55 MST 2016
Hi. I am trying to find an example for the ROM SPI control with DMA as stated in the user manual. The example a nice but it uses variables and type defines that are not shown anywhere.

I have tried to write my own driver for the DMA control based on a UART example and had it almost working but no clock even though I pre-programmed the SPI interface variables the same way I have done on polled and interrupt driven modes.

Any help wold be great.

Thanks,
Charles
Labels (1)
0 Kudos
Reply
1 Reply

1,339 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply