LPC15xx LPCOpen v2.08c (Incremental) package released

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC15xx LPCOpen v2.08c (Incremental) package released

1,355件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sundarapandian on Wed Jun 11 18:02:02 MST 2014
An incremental LPCOpen release of v2.08c is available for LPC15xx platform. Visit the LPCOpen page to download the package, the list of changes are available at the history page.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,347件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by YOZHik on Wed Jul 16 12:53:52 MST 2014
CONFIG_SCT_nRG is defined as 15 in sct_15xx.h. Shouldn't it be 16?
0 件の賞賛
返信

1,347件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Wed Jun 11 19:17:26 MST 2014
Wow  :exmark:

Are issues, which has been posted here, intentionally or accidentally ignored?

That's really motivating...
0 件の賞賛
返信