LPC1549 Standard IO Pin Protection and Voltage Levels

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1549 Standard IO Pin Protection and Voltage Levels

1,548件の閲覧回数
jpacl
Contributor I

The datasheet states that a standard IO pin is 5V tolerant, when Vdd is above 2.4V.  Can a standard IO pin be connected to a 5V voltage rail through a 3k resistor during power up, providing a 1.6mA current source?

Can a standard IO pin, configured as an input, be connected to 1.6V voltage source, placing the input into an indeterminate state, the logic state of the input would not be used in this case?

Can a standard IO pin, configured as an analog input, be connected to a 5V voltage rail through a 3k resistor indefinitely, providing a 1.6mA current source?

ラベル(1)
0 件の賞賛
返信
1 返信

1,530件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi jpacl 

>>The datasheet states that a standard IO pin is 5V tolerant, when Vdd is above 2.4V. Can a standard IO pin be connected to a 5V voltage rail through a 3k resistor during power up, providing a 1.6mA current source?
Can a standard IO pin, configured as an analog input, be connected to a 5V voltage rail through a 3k resistor indefinitely, providing a 1.6mA current source?

Answer: No. the max input leakage current is several uA, So it can't provide 1.6mA current. see below screenshot from Datasheet.

ZhangJennie_0-1667886912460.png

 

>>Can a standard IO pin, configured as an input, be connected to 1.6V voltage source, placing the input into an indeterminate state, the logic state of the input would not be used in this case?

Answer: No, 1.6V input is a indeterminate state, we can't use its logic state.

Thanks,

Jun Zhang

0 件の賞賛
返信