LPC11u12 & nxpUSBLib v0.98b

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11u12 & nxpUSBLib v0.98b

1,126件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by norbiv8 on Sat Mar 08 12:07:09 MST 2014
Hi,

i would like to connect to PC as generic HID device with 11u12. The example code is working on the 11u12, but just with the HIDClient.exe which included to the example. With my .NET HID library isn't work (i can't write to the device). With MCP2210 my HID library work well. Is it possible to download the HIDClient source code? Or any idea what could be a problem?

By the way the nxpUSBLib HID example fit to the 11u12, but the new lpcopen isn't. I expected the new lpcopen will be better than the old libraries.

Thank you,

Norbert
ラベル(1)
  • USB

0 件の賞賛
返信
0 返答(返信)