LPC11c24 CAN in silent mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11c24 CAN in silent mode

1,142 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nickich on Mon Jul 13 08:57:01 MST 2015
Hello,

I want to be able to monitor the CAN traffic without acknowledging any messages, and at the same time to be able to send a message on the CAN bus.
Is this possible with LCP11C24?
What I'm reading on the datasheet is that I can monitor the traffic by setting it in 'Silent Mode'. In this mode it looks like all transmit functionality is disabled, so it seems I cannot send a message.
In 'Basic Mode' I can send a message, but the messages I'm monitoring gets accepted. Is there a way of monitoring messages without being acknowledged by the LPC11C24? ...maybe some play with the filters and masks...?
Labels (1)
0 Kudos
Reply
1 Reply

1,094 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nickich on Thu Jul 16 08:44:44 MST 2015
...is that even possible?
0 Kudos
Reply