LPC11c24 CAN in silent mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11c24 CAN in silent mode

1,150件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nickich on Mon Jul 13 08:57:01 MST 2015
Hello,

I want to be able to monitor the CAN traffic without acknowledging any messages, and at the same time to be able to send a message on the CAN bus.
Is this possible with LCP11C24?
What I'm reading on the datasheet is that I can monitor the traffic by setting it in 'Silent Mode'. In this mode it looks like all transmit functionality is disabled, so it seems I cannot send a message.
In 'Basic Mode' I can send a message, but the messages I'm monitoring gets accepted. Is there a way of monitoring messages without being acknowledged by the LPC11C24? ...maybe some play with the filters and masks...?
ラベル(1)
0 件の賞賛
返信
1 返信

1,102件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nickich on Thu Jul 16 08:44:44 MST 2015
...is that even possible?
0 件の賞賛
返信