LPC11U68 ADCs 2Ms/s

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11U68 ADCs 2Ms/s

1,655件の閲覧回数
bobbann
Contributor I

LPC11U68 ADCs claim to run at 2Ms/s, but I am seeing conversion times of >60 clock cycles at 48MHz (<1Ms/s). I'm running a SeqA with a single channel in Burst mode, with an IRQ handler in RAM reading results into a simple buffer. Can anyone point me at a code sample which can achieve the 2Ms/s. I've checked the clock divider is 0 and Vdda is 3.3V.

Cheers, Bob.

EDIT :

  I solved this issue using DMA. 2MHz was then achievable.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,510件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Bob,

    Thank you for your problem solutions sharing!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信