LPC11U67 changing the FLASHCFG - FLASHTIM more than once

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11U67 changing the FLASHCFG - FLASHTIM more than once

1,466件の閲覧回数
mattiadell_oca
Contributor II

Dear All,

I need to change the FLASHCFG register while my program is running. Is it possible or I have to set it once?

I'm using a LPC11U67.

Best Regards,

Mattia Dell'Oca

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 返信

1,274件の閲覧回数
Dezheng_Tang
NXP Employee
NXP Employee

If you want to raise the CPU clock, make the FLASHTIM value bigger first, then switch the clock to higher speed. If you want to lower the CPU clock, switch the clock to slower clock first, then make the FLASHTIM value smaller.

As long as you follow this order, everything should be fine.

0 件の賞賛
返信