LPC11U24 Receive complete interrupt not working with Board_system() library!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11U24 Receive complete interrupt not working with Board_system() library!

1,109 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mahendra_ms on Mon Dec 07 23:31:32 MST 2015
Hello community and NXP
I'm new comers at NXP cortex chip, but i'm very well familiar with ARM architectures (with ARM7(LPC2148))
before facing this problem I've load the example code provided by community for UART which seems good with my LPCXpresso board , as I'm able to transmit and receive the data through UART with my desires baud rate 

Right now I'm doing Reverse Engineering with one project which use LPC11u24, and I've add UART code which is being provided by community.
my transition section working good but I'm not able to receive string in its RXC isr(tx section is working by polling of THRE while rx has ISR as per community ex. code)

instead of using chip library I'm using Board library here!
Here is my code

int main(void)
{
bool LCD_initialized = false;
uint32_t CurrentDisplay = DISPLAY_DEFAULT_MESSAGE;
uint8_t LCDmessagebuffer[160];
uint32_t LCDScrollCount = 0;
uint32_t i, NDEFmessagelen;
extern uint8_t defaultstring[];
uint8_t Buttons = 0;

Setup(); 
}


void Setup()
{

 HAL_BSP_BoardInit();                                                    //Board init funtion                        
// Setup Pins on the micro-controller
SystemCoreClockUpdate();

/* NVIC is installed inside UARTInit file. */
    UARTInit(4800);
    #if AUTOBAUD_ENABLE
    LPC_USART->ACR = 0x01<<2;                         /* Auto Restart, UART mode 0 */
LPC_USART->ACR |= (0x01<<0);                        /* Start */
    while(!UARTAutoBaud );
UARTAutoBaud = 0;
UARTSend((uint8_t *)"Auto Baud detected\r\n\r\n", 22);

#endif
#if MODEM_TEST
  ModemInit();
#endif

  print_string("smart meter Reading\r\n");        //Sending Hello string


  // never leave this function
  while (1) {
  __WFE();
            }
  return 0;
}

//**********************************************************************************************************
/* Set up and initialize hardware prior to call to main */
void Board_SystemInit(void)
{
/* Setup system clocking and muxing */
SystemSetupMuxing();
SystemSetupClocking();
//SetPowerProfile();
}


/* Sets up system pin muxing */
STATIC void SystemSetupMuxing(void)
{
LPC_SYSCTL->SYSAHBCLKCTRL |= (1<<16);                                   //Enable clock FOR IO config. block
LPC_IOCON->PIO0[0] = IOCON_FUNC0 | IOCON_MODE_INACT | IOCON_DIGMODE_EN; // RESET pin
LPC_IOCON->PIO0[1] = IOCON_FUNC0 | IOCON_MODE_INACT | IOCON_DIGMODE_EN;// ISP pin
LPC_IOCON->PIO0[3] = IOCON_FUNC0 | IOCON_MODE_PULLDOWN | IOCON_DIGMODE_EN; // GPIO ... will be VBUS when USB enabled
LPC_IOCON->PIO0[4] = IOCON_FUNC1 | IOCON_DIGMODE_EN;// I2C standard mode
LPC_IOCON->PIO0[5] = IOCON_FUNC1 | IOCON_DIGMODE_EN;    // I2C standard mode
LPC_IOCON->PIO0[6] = IOCON_FUNC0 | IOCON_MODE_PULLUP | IOCON_DIGMODE_EN;  // GPIO ... will be USB_CONNECT when USB enabled
LPC_IOCON->PIO0[7] = IOCON_FUNC0 | IOCON_OPENDRAIN_EN | IOCON_MODE_INACT | IOCON_DIGMODE_EN; // RED LED
LPC_IOCON->PIO0[8] = IOCON_FUNC0 | IOCON_OPENDRAIN_EN | IOCON_MODE_INACT | IOCON_DIGMODE_EN; // GREEN LED
LPC_IOCON->PIO0[9] = IOCON_FUNC0 | IOCON_OPENDRAIN_EN | IOCON_MODE_INACT | IOCON_DIGMODE_EN; // BLUE LED

LPC_IOCON->PIO0[12] = IOCON_FUNC1 | IOCON_MODE_PULLUP | IOCON_DIGMODE_EN;  // SW1
LPC_IOCON->PIO0[13] = IOCON_FUNC1 | IOCON_MODE_PULLUP | IOCON_DIGMODE_EN;  // SW2
LPC_IOCON->PIO0[14] = IOCON_FUNC1 | IOCON_MODE_PULLUP | IOCON_DIGMODE_EN;  // SW3
LPC_IOCON->PIO0[16] = IOCON_FUNC1 | IOCON_ADMODE_EN   | IOCON_MODE_INACT | IOCON_FILT_DIS;  // Reference voltage: AD5
LPC_IOCON->PIO0[23] = IOCON_FUNC0 | IOCON_DIGMODE_EN  | IOCON_MODE_INACT;  // VCC_SW
LPC_IOCON->PIO1[19] = IOCON_FUNC0 | IOCON_MODE_PULLUP | IOCON_DIGMODE_EN  | IOCON_MODE_INACT;  // FD input
}


/* Setup system clocking */
STATIC void SystemSetupClocking(void)
{

#ifdef WDO
Chip_SYSCTL_PowerUp(SYSCTL_POWERDOWN_WDTOSC_PD);

LPC_SYSCTL->SYSAHBCLKCTRL |= (1<<15);  // enable clock to WDT block

Chip_Clock_SetWDTOSC(WDTLFO_OSC_4_60, 2);

LPC_WWDT->CLKSEL |= (1<<0);  // select watchdog oscillator

Chip_Clock_SetMainClockSource(SYSCTL_MAINCLKSRC_WDTOSC);

//#else  /* the IRC is enabled by default */
//Chip_Clock_SetSysClockDiv(1);
#endif

Chip_FMC_SetFLASHAccess(FLASHTIM_20MHZ_CPU);
SystemCoreClockUpdate();
}

void SetPowerProfile(void)
{
static uint32_t command[4], result[3];

rom = (ROM **)0x1FFF1FF8;
#ifdef WDO  /* the WDO is running at 4.6 MHz but is divided by two */
/****Call the set_power routine ****/
command[0] = 3;/* Current freq in MHz  */
command[1] = PARAM_LOW_CURRENT;/* Use the designated low current power mode  */
command[2] = 3;/* Change the set_power  */

#elif defined (IRC_4MHZ) /* the IRC is running at 4 MHz */
/****Call the set_power routine ****/
command[0] = 4;/* Current freq in MHz  */
command[1] = PARAM_LOW_CURRENT;/* Use the designated low current power mode  */
command[2] = 4;/* Change the set_power  */

#elif  defined(IRC_12MHZ) /* the IRC is running at 12 MHz */
/****Call the set_power routine ****/
command[0] = 12;/* Current freq in MHz  */
command[1] = PARAM_LOW_CURRENT;/* Use the designated low current power mode  */
command[2] = 12;/* Change the set_power  */
#endif

(*rom)->pPWRD->set_power(command, result);/*Apply new power profile  */
}


//*****************************************UART.c*********************************************************************************

/*****************************************************************************
** Function name:UARTInit
**
** Descriptions:Initialize UART0 port, setup pin select,
**clock, parity, stop bits, FIFO, etc.
**
** parameters:UART baudrate
** Returned value:None
**
*****************************************************************************/
void UARTInit(uint32_t baudrate)
{
#if !AUTOBAUD_ENABLE
  uint32_t Fdiv;
#endif
  volatile uint32_t regVal;
  UARTTxEmpty = 1;
  UARTCount = 0;

  NVIC_DisableIRQ(UART_IRQn);
  /* Select only one location from below. */
#if 1
  LPC_IOCON->PIO0_18 &= ~0x07;    /*  UART I/O config */
  LPC_IOCON->PIO0_18 |= 0x01;     /* UART RXD */
  LPC_IOCON->PIO0_19 &= ~0x07;
  LPC_IOCON->PIO0_19 |= 0x01;     /* UART TXD */
#endif
#if 0
  LPC_IOCON->PIO1_14 &= ~0x07;    /*  UART I/O config */
  LPC_IOCON->PIO1_14 |= 0x03;     /* UART RXD */
  LPC_IOCON->PIO1_13 &= ~0x07;
  LPC_IOCON->PIO1_13 |= 0x03;     /* UART TXD */
#endif
#if 0
  LPC_IOCON->PIO1_17 &= ~0x07;    /*  UART I/O config */
  LPC_IOCON->PIO1_17 |= 0x02;     /* UART RXD */
  LPC_IOCON->PIO1_18 &= ~0x07;
  LPC_IOCON->PIO1_18 |= 0x02;     /* UART TXD */
#endif
#if 0
  LPC_IOCON->PIO1_26 &= ~0x07;    /*  UART I/O config */
  LPC_IOCON->PIO1_26 |= 0x02;     /* UART RXD */
  LPC_IOCON->PIO1_27 &= ~0x07;
  LPC_IOCON->PIO1_27 |= 0x02;     /* UART TXD */
#endif

  /* Enable UART clock */
  LPC_SYSCON->SYSAHBCLKCTRL |= (1<<12);
  LPC_SYSCON->UARTCLKDIV = 0x1;     /* divided by 1 */

  LPC_USART->LCR = 0x83;            /* 8 bits, no Parity, 1 Stop bit */
#if !AUTOBAUD_ENABLE
#if FDR_CALIBRATION
if ( uart_set_divisors(SystemCoreClock/LPC_SYSCON->UARTCLKDIV, baudrate) != TRUE )
{
      Fdiv = ((SystemCoreClock/LPC_SYSCON->UARTCLKDIV)/16)/baudrate ;/*baud rate */
      LPC_USART->DLM = Fdiv / 256;
      LPC_USART->DLL = Fdiv % 256;
  LPC_USART->FDR = 0x10;/* Default */
}
#else
    Fdiv = ((SystemCoreClock/LPC_SYSCON->UARTCLKDIV)/16)/baudrate ;/*baud rate */
    LPC_USART->DLM = Fdiv / 256;
    LPC_USART->DLL = Fdiv % 256;
LPC_USART->FDR = 0x10;/* Default */
#endif
#endif
  LPC_USART->LCR = 0x03;/* DLAB = 0 */
  LPC_USART->FCR = 0x07;/* Enable and reset TX and RX FIFO. */

  /* Read to clear the line status. */
  regVal = LPC_USART->LSR;

  /* Ensure a clean start, no data in either TX or RX FIFO. */
  while (( LPC_USART->LSR & (LSR_THRE|LSR_TEMT)) != (LSR_THRE|LSR_TEMT) );
  while ( LPC_USART->LSR & LSR_RDR )
  {
regVal = LPC_USART->RBR;/* Dump data from RX FIFO */
  }

  /* Enable the UART Interrupt */
  NVIC_EnableIRQ(UART_IRQn);

#if TX_INTERRUPT
  LPC_USART->IER = IER_RBR | IER_THRE | IER_RLS;/* Enable UART interrupt */
#else
  LPC_USART->IER = IER_RBR | IER_RLS;/* Enable UART interrupt */
#endif
#if AUTOBAUD_ENABLE
    LPC_USART->IER |= IER_ABEO | IER_ABTO;
#endif
  return;
}

/*****************************************************************************
** Function name:UART_IRQHandler
**
** Descriptions:UART interrupt handler
**
** parameters:None
** Returned value:None
**
**
*****************************************************************************/
void UART_IRQHandler(void)
{
  uint8_t IIRValue, LSRValue;
  uint8_t Dummy = Dummy;

  IIRValue = LPC_USART->IIR;
  IIRValue >>= 1;/* skip pending bit in IIR */
  IIRValue &= 0x07;/* check bit 1~3, interrupt identification */
  if (IIRValue == IIR_RLS)/* Receive Line Status */    //(if interrupt is Available for line status)
  {
    LSRValue = LPC_USART->LSR;
    /* Receive Line Status */
    if (LSRValue & (LSR_OE | LSR_PE | LSR_FE | LSR_RXFE | LSR_BI))
    {
      /* There are errors or break interrupt */
      /* Read LSR will clear the interrupt */
      UARTStatus = LSRValue;
      Dummy = LPC_USART->RBR;/* Dummy read on RX to clear interrupt, then bail out */
      return;
    }
    if (LSRValue & LSR_RDR)/* Receive Data Ready */
    {
      /* If no error on RLS, normal ready, save into the data buffer. */
      /* Note: read RBR will clear the interrupt */
      UARTBuffer[UARTCount++] = LPC_USART->RBR;
      if (UARTCount == BUFSIZE)
      {
        UARTCount = 0;/* buffer overflow */
      }
    }
  }

  else if (IIRValue == IIR_RDA)/* Receive Data Available *****************///(Receive complete interrupt)
  {
    /* Receive Data Available */
     data[count]=LPC_USART->RBR;
 if( data[count]=='\n')
 {
 data[count]=NULL;
 count=0;
 print_string(data);
 print_string("\r\n");
 }
 else
 {
 count++;
 }
  }
  else if (IIRValue == IIR_CTI)/* Character timeout indicator */
  {
                                /* Character Time-out indicator */
    UARTStatus |= 0x100;/* Bit 9 as the CTI error */
  }
  else if (IIRValue == IIR_THRE)/* THRE, transmit holding register empty *************///(interrupt for transmit buff Empty)
  {
    /* THRE interrupt */
    LSRValue = LPC_USART->LSR;/* Check status in the LSR to see if
valid data in U0THR or not */
    if (LSRValue & LSR_THRE)
    {
      UARTTxEmpty = 1;              //if tx buffer is Empty then set the flag!
    }
    else
    {
      UARTTxEmpty = 0;
    }
  }
#if AUTOBAUD_ENABLE
  if (LPC_USART->IIR & IIR_ABEO) /* End of Auto baud */
  {
LPC_USART->IER &= ~IIR_ABEO;
/* clear bit ABEOInt in the IIR by set ABEOIntClr in the ACR register */
LPC_USART->ACR |= IIR_ABEO;
UARTAutoBaud = 1;
  }
  else if (LPC_USART->IIR & IIR_ABTO)/* Auto baud time out */
  {
LPC_USART->IER &= ~IIR_ABTO;
AutoBaudTimeout = 1;
/* clear bit ABTOInt in the IIR by set ABTOIntClr in the ACR register */
LPC_USART->ACR |= IIR_ABTO;
  }
#endif
  return;
}


All help and comments welcome
Thanks and Regards,
Mahendra Sondagar


Labels (1)
0 Kudos
Reply
0 Replies