LPC11E68JBD64_SPI_LSB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11E68JBD64_SPI_LSB

1,471 Views
shenjian
Contributor II

I use LPC11E68JBD64_SPI ,I can't config the SPI serial data transfers start with the least significant bit. please help me.

Tags (1)
0 Kudos
Reply
1 Reply

1,404 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Yao,

Yes, SPI of the LPC11E68 is always MSB first, it can not be LSB first>

There is NOT a register to select the MSB first or LSB first for LPC11E68, the default is MSB first.

BR

XiangJun Rong