LPC11E68 build error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC11E68 build error

跳至解决方案
3,792 次查看
lajostoth
Contributor II

Hi,

I am using LPCXpresso IDE and LPCopen 2.12 11E68 example projects.

I have met build errors with all projects.

 I am seeking help for what is the reason of this errors?

0 项奖励
回复
1 解答
3,190 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

For LPC11E68 you should use the LPC116Ex wizard from the "Quickstart Panel - New project" option and select LPC11E68 explicitly. For more details please read the LPCXpresso IDE User Guide supplied built into the product.

You will need to import the LPC11U68 LPCOpen package though (the LPC11E6x family is basically the same as LPC11U6x but without USB support).

With regards to the error message, I suggest you look at: Linker Error "cannot find -l<lib_name>" 

Regards,

LPCXpresso Support

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,189 次查看
lajostoth
Contributor II

Hi!

 There are some problems in both the 11U68 2.12 LPCOpen library and the 11E68.

There is type conflict error with pinMask function arguments in the gpio_11u6x c and h files.

lpc1.PNG

I think it should be uint32_t pinMask.

-Missing closing brace for function in syscon_11U6x.c file:

lpc2.PNG

Best regards

3,191 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

For LPC11E68 you should use the LPC116Ex wizard from the "Quickstart Panel - New project" option and select LPC11E68 explicitly. For more details please read the LPCXpresso IDE User Guide supplied built into the product.

You will need to import the LPC11U68 LPCOpen package though (the LPC11E6x family is basically the same as LPC11U6x but without USB support).

With regards to the error message, I suggest you look at: Linker Error "cannot find -l<lib_name>" 

Regards,

LPCXpresso Support

0 项奖励
回复
3,190 次查看
soledad
NXP Employee
NXP Employee

Hi,

It is necessary to import the LPCOpen Chip Library for the device used and optionally the LPCOpen Board Library Project. For do that it is necessary to follow these steps:

 

1. Click on Import project(s).

pastedImage_3.png

 

2. Select the examples archive file to import. In this case, the projects imported are contained within archives .zip. 

pastedImage_4.png

 

3. For this example the LPC11U14 LPCXpresso board is selected. Click Open. Then click Next

pastedImage_5.png

 

4. Select only the LPCOpen Chip Library and LPCOpen Board Library Project. Click Finish.

pastedImage_6.png

 

The same steps are required for any LPC device and board you are used.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,190 次查看
lajostoth
Contributor II

Thanks for help!

I followed these steps based on tutorial:

https://community.nxp.com/docs/DOC-333169

but I used 11e68 library.

I get the same result with initial source code.

Lpc11e68_2.PNG

0 项奖励
回复