LPC11C24

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC11C24

3,104 次查看
ianbenton
Senior Contributor I

Having just designed in the LPC11C24, I was suriprised that Mouser was listing it as "end of line".

I checked the NXP website, and the LPC11C family was listed as containing 20-pin TSSOP devices and 33-pin HVN devices - when I designed in the LPC11C24 I was hoping for a device with fewer pins, so no problem so far, but I was puzzled how it would manage "up to 42 GPIO".

So I checked the datasheet, and the only devices listed are the original 48 pin devices that I was trying to buy but told they were obsolete.

Please explain.

0 项奖励
回复
4 回复数

3,084 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

As you mentioned the only devices available are the 48 pin devices. Could you please clarify where did you see LPC11C24 listed as 20 and 33 pin package?

Regards,

Felipe

0 项奖励
回复

3,066 次查看
ianbenton
Senior Contributor I
0 项奖励
回复

3,052 次查看
FelipeGarcia
NXP Employee
NXP Employee

Thank you for the clarification.

I checked this internally and the LPC11C24 being listed as 20 and 33 pin package is a mistake in our website. I will report this to the web team.

Also I verified that LPC11C24 is still active, you can check any quality notifications for this device in the NXP Customer Support community if you register to this page.

https://extranet.nxp.com/pcn/private/index.html

Best regards,

Felipe

0 项奖励
回复

2,989 次查看
ianbenton
Senior Contributor I

Mouser has just sent another e-mail saying it is “end of life”.

can you still confirm that it is active?

0 项奖励
回复