LPC11C14FBD48 in LPC Initialization Tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11C14FBD48 in LPC Initialization Tool

1,727件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhd on Mon Feb 01 14:58:43 MST 2016
Hello,

LPC11C14FBD48 is not available in LPC Initialization Tool?


Best regards
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,681件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Feb 02 12:30:46 MST 2016

Quote: Javier.Hernandez
Sorry, I did not know they were old parts.



... so a better choice is a LPC15xx  ;-)
0 件の賞賛
返信

1,681件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jhd on Tue Feb 02 08:34:13 MST 2016
Hi!,

Sorry, I did not know they were old parts.

I changed the LPC54102 for LPC11C14 (to use with the CAN transceiver of the MC33908NAE) because I need at least one CAN controller. I had to remove some other device, or change the way of communication, but I hope that this will be sufficient for my needs. 1 x UART RF module, 1 x SPI to MC33908NAE, 1 x CAN controller to built-in CAN transceiver of the MC33908NAE, 1 x I2C and a few GPIO.

Best regards
0 件の賞賛
返信

1,681件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Feb 02 00:30:30 MST 2016
Please refer to our previous response - the situation with older LPC11 family parts is the same as the LPC12 family that you asked about previously ...

https://www.lpcware.com/content/forum/lpc122x-lpcinit-tool#comment-1149296

Regards,
LPCXpresso Support
0 件の賞賛
返信