LPC1115 code doesn't run after power cycle

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1115 code doesn't run after power cycle

2,808件の閲覧回数
kwat100br
Contributor I

I have an LPC1115 development board and can debug and upload code as you would expect.

I can disconnect a debug session and the code is running. 

If I unplug the MCU in again it will not run the code. It lights the on board rgb LED a color (not sure if if its the same color each time, I think it is).

Here is the project repo.

We have never been able to get the board to power on and run the code.  This is a big deal. Does the processor need to be reset? Or is the code not uploaded properly?

Running Windows 10 MCUExpresso IDE Latest version

Running Ubuntu 16.04 LTS MCUExpresso IDE Latest version

Thank you!

Kevin

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,661件の閲覧回数
converse
Senior Contributor V

It looks like you are using the Semihost library variant - this requires a debugger connection. Suggest you change to a NoHost library:

Switching the selected C library 

https://community.nxp.com/thread/389153 

0 件の賞賛
返信

2,661件の閲覧回数
kwat100br
Contributor I

Some one else mentioned about flash and ram and that the linker/loader I Was using was putting it at ram and not flash, I do not believe this is the case. I didn't notice your links you provided. I will hopefully get access to the board soon to try again.

thank you. This is still open. converse‌

0 件の賞賛
返信