LPC1113 /202

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1113 /202

Jump to solution
1,888 Views
SkyPilot
Contributor I

Hello, We are an aviation company that uses the LPC1113 /202 controller in our instruments. We needing to source a module / socket with pins so we can access so we can program the chip in ISP mode.

 

Any help would be appreciated.

Labels (1)
0 Kudos
Reply
1 Solution
1,810 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @SkyPilot,

The following debuggers support LPC1100

Universal Multilink Development Interface | NXP Semiconductors

PEmicro Cyclone FX programmer | NXP Semiconductors

Universal Multilink FX High-Speed Development Interface | NXP Semiconductors

PEmicro Cyclone programmer | NXP Semiconductors

You can refer to the connections on the following board, which supports the LPC1100 series:

LPCXpresso1125 Board | NXP Semiconductors

Additionally, according to Section 6.2: Pin Description in the datasheet, a LOW level on pin PIO0_1 during reset triggers the ISP command handler.

Best Regards,

Pablo

View solution in original post

0 Kudos
Reply
2 Replies
1,789 Views
SkyPilot
Contributor I

Thank you Pablo,

 

This should get me on the right track.

0 Kudos
Reply
1,810 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @SkyPilot,

The following debuggers support LPC1100

Universal Multilink Development Interface | NXP Semiconductors

PEmicro Cyclone FX programmer | NXP Semiconductors

Universal Multilink FX High-Speed Development Interface | NXP Semiconductors

PEmicro Cyclone programmer | NXP Semiconductors

You can refer to the connections on the following board, which supports the LPC1100 series:

LPCXpresso1125 Board | NXP Semiconductors

Additionally, according to Section 6.2: Pin Description in the datasheet, a LOW level on pin PIO0_1 during reset triggers the ISP command handler.

Best Regards,

Pablo

0 Kudos
Reply