LPC USB device Detection to Host PC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC USB device Detection to Host PC

905件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by venkatesh on Thu Feb 14 02:31:21 MST 2013
Hi,

I am working on LPC1768 baord.
If i use mass storage firmware, this board is able to detect as LPC MASS STORAGE device in windows7/xp.

1. Now i am trying to make board as similar functions as custom device of USB class (client usb device) and should detect this board as their device in HOST(windows PC)..
So, Now i am able to map descriptor information in LPC as provided as custom USB device.(checked with USB analyzer tool).i hope during the enumeration time these will fetch by HOST and able to detect this LPC device as their Custom USB device. But its not happening.


Any one suggest me to check if i miss any thing to detect the device.

Thanks,
Venkatesh
ラベル(1)
0 件の賞賛
返信
0 返答(返信)