LPC-Link2 with LPC55S0X

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-Link2 with LPC55S0X

ソリューションへジャンプ
2,297件の閲覧回数
Jack_Star-int
Contributor I

I am working on a custom made board with LPC55S06/LPC5506 MCU. 

We have LPCXpresso55S06 EVK but we want to explore if LPC-LINK2(OM13054) could be able to work with MCUExpresso to debug and download firmware to the internal flash of our custom board. 

 

0 件の賞賛
返信
1 解決策
2,284件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Jack_Star-int,

As it mention in the LPC-Link webpage, the LPC5000 family is supported. The webpage still doesn't add the LPC550x but is from the same family.

Best Regards,
Alexis Andalon

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,284件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Jack_Star-int,

As it mention in the LPC-Link webpage, the LPC5000 family is supported. The webpage still doesn't add the LPC550x but is from the same family.

Best Regards,
Alexis Andalon

0 件の賞賛
返信
2,274件の閲覧回数
Jack_Star-int
Contributor I

Hi @Alexis_A ,

Thanks for your explanation. I will get the LPC-Link and have it tested with my custom board.

Thanks,

Jack.L

0 件の賞賛
返信