LPC-Link2 speed?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,756件の閲覧回数
danielholala
Senior Contributor II

Hello,

I'd like to know the speed of the LPC-Link2 debug probe but could not find any information about it.

Especially, what is

  • download speed into RAM
  • max. target interface speed
  • max. SWO speed

Segger provides a nice chart providing this information for the J-Link probes here.

Gathering this information facilitates comparison of different probes.

Thanks.
Dan

0 件の賞賛
返信
1 解決策
2,735件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

 

Hello danielholala, 

After confirm with internal, share the below information:

 

LPCLink2 use HS USB, and maximum SWD speed is about 4MHz

  • download speed into RAM: ~50KB/s
  • max. target interface speed: you mean SWD clock speed? ~4MHz.
  • SWO speed: ~4Mh

 

Hope it helps,

 

Alice

元の投稿で解決策を見る

2 返答(返信)
2,735件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

 

Hello danielholala, 

After confirm with internal, share the below information:

 

LPCLink2 use HS USB, and maximum SWD speed is about 4MHz

  • download speed into RAM: ~50KB/s
  • max. target interface speed: you mean SWD clock speed? ~4MHz.
  • SWO speed: ~4Mh

 

Hope it helps,

 

Alice

2,724件の閲覧回数
abnxpweb
Contributor III

Given that on many devices you can get flash programming speeds way in excess of the speed you quote for writing to RAM, I suspect your figures are somewhat out!

0 件の賞賛
返信