LPC LINK2 heating

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC LINK2 heating

1,357件の閲覧回数
namdeopatil
Contributor I

I am using TWO LPC LINK2 for debugging PN7462.

I have Two different PN7462 hardware boards.

I also have One PN7462 EVM

When we test these using LPC LINK2.

The LPC LINK2 gets heated within 10-15 minutes.

I have tried both the LPC LINK2, both get heated in 10-15 minutes.

What could be wrong ?

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,224件の閲覧回数
driesmoors
NXP Employee
NXP Employee

Nothing is wrong. This looks like normal behavior: I experience the same, regardless of the board attached to it. I guess the debugging protocol firmware running on the LPC-Link2 boards is designed with performance in mind, and nothing else.

0 件の賞賛
返信